Change Language :

Winner of the green vector award 2022: Dercks Gartenbau GmbH designed the precision watering trolley with the aim of conserving groundwater resources and saving energy costs. After a successful first prototype, the second model with a span of 45 metres has now been designed for the targeted irrigation of potted plants over an area of 9,190 m2. To ensure that the supply lines and the two hoses for the water supply are not dragged across the ground, they run safely above it in an energy chain. Intelligent sensor technology for measuring push and pull force supplements the energy supply.
"To achieve maximum space utilisation on the footprint of the precision casting trolley, the energy chain is a must. The investment in the energy chain is amortised in four years thanks to the additional floor space gained. We are therefore pleased to be able to use the energy chain here."
Peter Dercks, Dercks Gartenbau GmbH
In person
Monday to Friday: 8 am – 8 pm
Saturday: 8 am – 12 pm
Chat-Service
Monday to Friday: 8 am – 4 pm
WhatsApp-Service
Monday to Friday: 8 am – 4 pm